This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN75LVCP600: signal polarity and the place of this device

Part Number: SN75LVCP600


Hi team,

I have two questions.

1. SATA signal polarity should be matched with SN75LVCP600 Rx/Tx polarity? 

e.g.

SATA + is connected to RX+

SATA - is connected to RX-

2. The datasheet mentions that the device should be placed within 6mil to RX. 

If the distance is closer than 6mil, is this more helpful for the equalize function? or almost same performance even if the distance become closer than 6mil?

BTW, the unit of <6 " of figure 9 in the datasheet is mil, right?

Regards,

Noriyuki Takahash