Part Number: LM1117
Other Parts Discussed in Thread: TLV1117
Hello Again.
I have a LM1117 MP-2.5, that operates with a temperature range, from 0 °C to 125 °C.
I need a device with the LM1117 I MP part number with the Vout = 2.5 V that operates with a temperature range, from -40 °C to 125 °C, but i can't find it.
Please, could you help-me to find one ?
I need the same footprint / pinout / Vout = 2.5V / Temp. Range = -40 °C to 125 °C.
Thanks in advance
Angelo Silva - Brazil