Part Number: TPS25810
Other Parts Discussed in Thread: HD3SS3212, , TPS2546, TPS2514
Could you inform communication fail mechanizm?
We use TPS25810 by USB VBUS line and HD3SS3212 by USB communication line from SoC.
We have a trouble that our product can't communicate to iPhone when TPS25810 is set CHG=CHG_HI =1(it is 3A setting),
however it can communicate to iPhone when TPS25810 is set CHG=1, CHG_HI=0(it is 1.5A setting) .
I found following article, it is written that it can't communicate 5V/3A.

But I'd like to know mechanizm why can't communicate
(e.g, what data does TPS25810 send via CC line to iPhone? then what is set inside iPhone?, etc).
And do you have solution to communicate with iPhone at 5V/3A setting(CHG=CHG_HI=1)?