This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB1210: can we use TUSB1210+ level shifter to achieve 3.3V ULPI?

Part Number: TUSB1210

Hi,

we are trying to replace USB3320 with TUSB1210, but the ULPI is 3.3V in the customer's system.

Can we add level shifter to overcome the voltage incompatibility?

If yes, which level shifter is recommended?

What's the IO type of ULPI, is it push-pull or open drain or something else?