Part Number: TCAN1042V-Q1
Hello,
my customer is currently doing a design with the TCAN1042V-Q1 and he would like what the specified bus fault protection exactly stands for (+-70V & +-58V)? is refering to the DC voltage that the bus pins can handle without being damaged or is it refering to something else?
Also he would like to know if the thermal pad under the VSON Package has to be connected to the GND pin? (i think it doesn't).
Best regards,
Stani