Part Number: TPS65987D
Other Parts Discussed in Thread: TPD6S300A
we have two TPS65987D. One of them is shall sink 20V 3A starting from dead battery. I have connected ADCIN1 to a 130k/100k voltage divider (DIV=0.43) and a pulldown on the MISO line. This should make the PD-controller to select BP_NoWait and Configuration 3. Connecting an USB-C cable to a power source that can deliver 20V 3A gives only 5V. Doing the same thing with a TPS65987-90 Evaluation Module gives 20V. (S4 sw5 on, and pressing S3 while connecting the USB cable.)
There are two differences in the designs:
1) On our board there is a TPD6S300A for protection,
2) On the Eval-board the PD-controller is PTPS65987D, on our board is a released TPS65987D.
Is there any difference between the two versions of TPS65987D that can explain the different behavior?
Connecting USB cable to our Board gives 5V 0.10A. (Packet 18: Request Obj Pos 1.)
Connecting USB-cable to TPS65987-90 Eval Module while pressing S3 gives 20V 3A. (Packet 22: Request Obj Pos 6.)
Is there anything we can try? we have two TPS65987D.docx