Part Number: SN65HVD251
Other Parts Discussed in Thread: STRIKE
Dears,
We are using IC SN65HVD251D in our designs.
We are facing issue of IC getting short VCC to GND (VCC and GND pins are observed shorted together).
We are observing this problem repeatedly.
IC SN65HVD251D is operating on 5VDC.
Also IC output is protected from tvs diode.
Please note that the we have cable length of about 30 meter long which carries 24VDC and from this 24VDC we have generated 5 VDC using DC to DC converter LM2672M_ADJ.
This power supply is also protected with transorb, ferrite bead in series with output and input and output capacitor filters.
Can you please help us to identify;
Possible causes of IC damage?
What are the parameters which can damages the IC?
Preventive measure and circuit protection guidelines?
Types of Measurements in filed to find out the root causes?
Design support for robustness improvement to avoid failure?
Please see attachment for the IC damage images