Part Number: SN65C1167E
Dears,
Communication between boards using SN65C1167EPW.
Under certain conditions Receive abnormal data.
When I investigated it,
it was in the state of the attached file(schematic-SN65C1167EPW.jpg ).
(Abnormal data occurs when SW1 is ON.)
Below are the questions.
Q1.In the attached circuit diagram, when SW1 is ON,
What waveforms are received on 1R and 2R of IC-B.
Q2.Actual 1A and 2A became like the attached oscilloscope waveform(OscilloscopeWaveform.jpg).
Is it as expected?
When the 1D and 2D logic of IC-A is in the attached file(schematic-SN65C1167EPW.jpg ) state,
(IC-A 1D is Drive-L,IC-A 2D is Drive-H)
Pulses such as 90deg phase difference pulses continuously enter the IC-B side.
(The counter circuit after IC-B counts.)
However, if the combination is different from the attached file(schematic-SN65C1167EPW.jpg ) state,
(IC-A 1D is H,2D is H. IC-A 1D is L,2D is L. IC-A 1D is H,2D is L.)
It does not become a pulse like a 90 ° phase difference pulse.
(The counter circuit after IC-B does not count.)
Q3.Why is the attached file(schematic-SN65C1167EPW.jpg ) combination
Will continuous 90 ° phase difference pulses be output?
Best regards,
Kanetomo Nozaki