Part Number: ADS1256
Hi Team,
I want to switch the multiplexer and read the following data.
Ch.1 (6 significant digits) Data integration time 100ms
Ch.3 (5 significant digits) Data integration time (T.B.D : ex.50ms)
Measured against analog value 0V.
Acquire Ch1.Ch2 alternately 5 times per second.
Below are the questions.
(1) Since Ch.3 has fewer significant digits than Ch.1, is it okay to shorten the data acquisition time?
(I understand that there is no problem when I look at Figure.19)
(2) Is it necessary to wait for stabilization when Ch.1 and Ch.3 have different input values?
(For example, when Ch. 1 = 2 V, Ch. 3 = 0.1 V is input)
(3) Is it good to understand that if the measurement is performed while switching between Ch.1 and Ch.3,
fluctuations in the value of Ch.3 during integration of Ch.1 will not affect the data of Ch.3 after switching?
(According to Figure.19, it seems that data is accumulated after switching by Multiplexer.)
Best Regards,
Kenji