Part Number: PCA9544A
Other Parts Discussed in Thread: TCA9548A, TCA9544A
I’m looking for a part like the PCA9544A with 8 channels instead of 4. Do we have anything like that?
Mux should support a chip reset and indivdual channel interrupts
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hey Saminah,
Unfortunately not. The only 8 channel switch we offer are the PCA/TCA9548A which do not have the INT channels we need.
The only alternative solution I can think of is to use 2 TCA9544A's or a TCA9548A with some kind of OR gate or an 8 bit I/O expander.
Thanks,
-Bobby