Part Number: DP83848-EP
Hi Guys,
Troubleshooting a board having the DP83848-EP PHY on it and which refuses to complete a file transfer. Other sibling boards pass, so something defective (PHY, MAC FPGA, or PWB).
- PHY successfully configured by FPGA and then passes Internal and External Loopback
- Scoping PHY signals reveal no stuckies:
- Wireshark detects SYN Req from client, followed by SYN ACK from FTP Server, but no ACK back from Client, so not sure Client received the SYN ACK from server and so the file transfer times out
- Observed that RX_ER, pin 41, pulsed high at the beginning of the attempted FTP (2us wide pulse).
- What does it mean, given that the PHY passed EXT loopback?
- What is the definition of False Carrier Sense? When reading Reg#10 (PHYSTS) bit11 is set. Does it mean bad RX signals from the isolation Xformer? But ext loopback passed continuously..
Appreciate any help
Thanks,
D.J