Part Number: SN65DP159
Hello team,
my customer wants to use the SN65DP159RS in a SMARC module, since the SMARC standard states that the DDC signals are 1.8Vdc and that the translation from 1.8Vdc to 5 Vdc must be made on the carreir (not on the SMARC module), I wanted to ask you if it is possible NOT to connect the DDC lines or if it is possible to connect them to a 1.8V level or if there is a further solution.
Thank you in advance for the support.
Best regards,
Adrian