Part Number: DS90UB953A-Q1
Hi Sir,
Please kindly advise which one is correct on UB953 POC circuit, thanks.
Fig.1
Fig.2
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB953A-Q1
Hi Sir,
Please kindly advise which one is correct on UB953 POC circuit, thanks.
Fig.1
Fig.2
Ian,
the figure1 is used for low back channel data rate, such as UB933/ub934/UB964 link, figure2 is designed for higher FC/BC rate such as ub953/954 combo.
for your design, pls check the link FC and BC rate setting (this can be set based on your system design through the reg.), if the BC is over 25Mbps, figure2 is better.
best regards,
Steven