This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65987EVM: Compatibility of TPS65987EVM

Part Number: TPS65987EVM

Hi team,

Customers have the following questions:

1. Customers use TPS65987-90EVM + 10G-EXPANSION-EVM board. The output of computer Type-C port is connected to the display through DP interface on sink board. Testing Huawei two computers, Dell two computers, MacBookpro computer have picture output, and Millet two computers have no picture output. Confirm that the type-C port of millet computer can output DP signal (because connecting other DP to HDMI docks can display pictures). Is there compatibility problem and how to verify or adjust it?

2. Samsung Galaxy S8 mobile phone with DP ALT MODE, can it directly access the Type-C port to display? (Connecting DP TO HDMI dock can also be displayed)

ps:TPS65987-90EVM:http://www.ti.com.cn/cn/lit/ug/slvubf3a/slvubf3a.pdf

Could you give some suggestions?

Best Regards,
Amy