Part Number: TRS232E
Other Parts Discussed in Thread: MAX202, , TRS232
Hi Tiers
i use the max202 in my project, but it shouldn't be the optimal solution,
Can the TRS232/TRS232E replace the MAX202?
Is there any other P/N recommended, need Pin to Pin
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Jack,
Yes, TRS232 or TRS232E can pin 2 pin replace MAX202. All devices are 5V RS-232 transceivers. TRS232E comes with 8kV IEC contact ESD protection. The few difference is:
| data rate | output voltage | cap | |
| TRS232 | 250kbps | 7V | 1uF |
| MAX202 | 125kbps | 9V | 0.1uF or 1uF |
Please let me know if you have more questions.
Regards,
Hao