Part Number: TPS65982
Hi team,
I am working on bringing up a TPS65982 and configure it to sink 15V. However, the controller's I2C lines are routed through an FPGA. Basic idea was to configure the FPGA as I2C master and then configure the controller through the FPGA. But, there is a defect in the FPGA circuit, which renders the FPGA unprogrammable.
Question:
1. Can you please help us that how can we program this controller other than using the I2C pins of the controller?
2. Correct me here if I am wrong, that the initial configuration is loaded from the SPI flash. So is it possible we program the flash memory instead?
Best
Sid