Part Number: DS90UB960-Q1
Hello team,
We are considering a design with customer using 960+953 and had below questions:
- Is there a way to have PDM mic data in the same line? I'm not finding anything in this regard
- How much power can we drive through coax with POC? What is the max power draw (peak and steady)?
- If there is a separate I2C interface for each camera, and if there are 4 FPD interfaces and 2 I2C interfaces, how would that work? There will also be a few other non-camera I2C devices on this line--> What I understand is that the secondary I2C line on 960 is only recommended to be used if there are two host processors (rather than trying to address each camera individually). I see this app note (http://www.ti.com/lit/an/snla222/snla222.pdf) but am still not quite sure how it would apply to 960 since there is one DES address.
Thanks!