Part Number: TPS25810
Other Parts Discussed in Thread: TPS2514, TPS2546, TPS65987D
Hello
Customer use TPS25810 EVM used below tool then test Apple mobile phone. It shows only support 2.4A charging. Is it correct?
1.Below is customer schematics. They connect to different mobile phone but still can not charging 5V up to 3A. Could we know what is the issu root cause?
2. Type C Dp/Dn pin is connected to CPU and TPS2514 Dp/Dn simultaneously on schematics.
First condition: if de-pop CPU Dp/Dn connection and type c connector Dp/Dn connect to TPS2514 , it can charge Millet mobile phone to 1.6A but can not access USB 2.0 device by external Typec HUB.
Second condition: If de-pop TPS2514 Dp/Dn and type c connector Dp/Dn connect to CPU USB 2.0 , the board can not support fast charge but can access USB2.0 device by external Typec HUB.
Could we know how to support fast charge 5V/3A and access USB2.0 device simultaneously ?
BTW, That is NB application. Customer see many mobile phone support QC2.0/QC 3.0 and less find support BC1.2 mobile phone. How to implement QC 2.0/QC 3.0 5V/3A and which PD solution support it? Thank you.
BR
Patrick