Part Number: DS90CR286A
Hi Team,
Customer is using DS90CR286AMTD to convert camera_link to RGB, and finds that the RGB receiver can not detect the correct resolution.
The input signal of camera_link camera is 640*512 and the frame rate is 50fps.
After the chip works, it is found that the VSYNC signal is 50 hz, the HSYNC signal is 26.32 kHz and the DE signal is always high.
Questions:
1. Is it normal that DE signal is always high?
2. For input signal 640x512 50fps, what is the correct frequency value of the converted Vsync and hsync?
Here is the schematic:
Best Regards,
Amy Luo