Part Number: SN65DSI86
Hi Team,
The customer is using DSI86, and the screen resolution is 2560x1440. For diff application, they like to switch the refresh rate of the screen between 60Hz and 90Hz. But they want to switch it very fast, hoping the user can not see the dark screen. So they are asking what is the fast operation of the refresh rate update, and how fast could it be?
Best Regards,
Peter Wei