Can anyone tell me if AC coupling caps are required to be used on the high speed inputs to this CML repeater? The datasheet does not explicitly require them, although I see a cartoon that uses such caps on both the inputs and the outputs of the part.
I am operating at about 1.44 Gbps and am wondering if I should stop and modify a current board fabrication that does not incorporate such AC coupling (or "DC blocking") caps on the high speed inputs.
Thanks.