Part Number: DS100BR410
Can anyone tell me if AC coupling caps are required to be used on the high speed inputs to this CML repeater? The datasheet does not explicitly require them, although I see a cartoon that uses such caps on both the inputs and the outputs of the part.
I am operating at about 1.44 Gbps and am wondering if I should stop and modify a current board fabrication that does not incorporate such AC coupling (or "DC blocking") caps on the high speed inputs.
Thanks.