Part Number: DS25CP102
Hi Team,
I received the following request:
My customer is using 2 ds25cp102 and they want to be able to configure them in all possible ways, even with regards to equalization and pre-emphasis.
To reduce the dimensions of the components they want to use the pull-downs that are in the chip by putting the jumpers on the outside towards VCC
If they configure the pin to '1', but the pulldowns are 20k they are afraid that 20k ohm are weak if the pin is left open!
Can you comment on it?
Regards,
Fabio