Part Number: DP83825I
Hello TI,
1. What is the input capacitance of the XI pin in RMII Slave Mode? Is this really still 15pF / 30pF (typ / max) in this mode?
2. Table 86 in the datasheet (snls638a) says "LED_2 Control:Selects the source for LED_1". Is this a typo?
3. The datasheet refers to led_1 on numerous occasions. Which pin is led_1 available on in this part?
4. Page 7 of the datasheet specifies the bootstrap characteristics as having similar V_IH (1.3V) and V_IL (0.6V) levels at 1V8 and 3V3, while Table 7-2 on page 39 specifies 0.7 x VDDIO and 0.35 x VDDIO respectively. Which of the two is correct?