Part Number: DS90UB954-Q1
Other Parts Discussed in Thread: ALP, USB2ANY
Hi team,
We have the problem of not being able to connect to the board created by ALP.
We want to control 954 on the prototype board with ALP using USB2ANY.
First, I was able to confirm that I could access EVM 954.
However, we do not have access to 954 on our board.
It is displayed as unknown FPD-LINK deserializer on ALP.
There are two differences between EVM and our board.
1. The 954 ID on our board is not default.
I think that the device should be recognized even if the ID is changed.
Is it correct?
2. The 954 I2C is not directly, but via the MCU.
954 <=I2C=> MCU <=I2C=> USB2ANY
Is there a possibility that Des cannot be recognized if I2C is relayed in this way?
Best regards,
Tomoaki Yoshida