Part Number: DS125DF1610
Other Parts Discussed in Thread: DS280BR820EVM, LMX2581, DS280BR820, SIGCONARCHITECT, , DS280DF810EVM, DS280DF810, DS250DF810
Hello Team,
My customer are going to use DS125DF1610 in their new project and asked several questions.
Currently they have DS280BR820EVM board and are going to test logic and ability to run BERT.
As described in 12-Gbps BERT Board Reference Design(DS125DF1610) - to launch BERT it needs to connect LMX2581 to input of one of the channels.
1) What frequency should be on that input of DS280BR820 and what setting should they use to run at 10.3125 Gbps?
2) Do they understand correctly, that it need to use a separate group of channels for generation and a separate group of channels to test PRBS?
3) It is clear that the Error Count (bit) is read from the chip by the registers Reg_0x83 [2: 0] = prbs_err_cnt [10: 8], Reg_0x84 [7: 0] = prbs_err_cnt [7: 0].
How does Error Rate (bits/min) and Bit Count calculated in SigConArchitect?
Thank you in advance!
BR,
Ilya