Part Number: TIOL111
I want to use TIOL111 in my design. i want to derive L+ and L- internally of my PCB and only i want to expext CQ externally. Can i do like this or not ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TIOL111
I want to use TIOL111 in my design. i want to derive L+ and L- internally of my PCB and only i want to expext CQ externally. Can i do like this or not ?
Yes, that's right. You system can just receive the CQ line; it doesn't need L+/L- supplied externally as long as they can be generated somehow.
If L- doesn't connect to the system that is providing CQ, though, you should be careful about potential differences between that system's ground and L-, since this could cause apparent shifts in the voltage on CQ.
Regards,
Max