Part Number: AM3358
Other Parts Discussed in Thread: TUSB4041I, , TS3USB30E, TPS65218
We intend to design a PCB containing a USB High Speed hub TUSB4041I where
one of the ports are connected directly to an AM3358 USB port configured as a device.
The AM3358 is powered from a backplane, which might be powered down
The USB hub is self-powered, but will also get power from the backplane if present.
Are the USB pins on the CPU protected?
We are worried about what happens if the CPU is powered down, and the USB hub is not.
Is there a problem with latchup or other problems which might affect long time reliability?
Best Regards
Ulf