Part Number: TDP158
Hi Team
Does TI TDP158 support 4K2K@60Hz(YUV 4:2:0) input / output ?
The HDMI source from CPU and outpuy type is AC coupled
Can I use TDP158 for AC coupled to DC coupled level shift function ?
Competitor : ASM1442K
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TDP158
Hi Team
Does TI TDP158 support 4K2K@60Hz(YUV 4:2:0) input / output ?
The HDMI source from CPU and outpuy type is AC coupled
Can I use TDP158 for AC coupled to DC coupled level shift function ?
Competitor : ASM1442K
Kerr
Similar parts would be DP149 (Retimer) or DP139 (Redriver) since you don't need the HDMI2.0.
Please note the TDP158 does not have Adapter ID buffer for HDMI.
Thanks
David
Hi David
Can TI DP159/DP139 support level shift function like ASM1442 ?
Web : www.asmedia.com.tw/.../e_show_products.php
Customer need ASM1442 function + redriver
Kerr
Can you please confirm that the ASM1442 input accepts DP++?
The ASM1442 says converting low-swing AC-coupled differential input from existing PCI Express in the chipset of PC to HDMI compliant differential output. But the block diagram of the ASM1442 does not show any bridge functionality, just a level shifter.
If it is a DP++ to HDMI level shifter, then DP139 can support as well.
Thanks
David