This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65DSI86: how to use DSI_CLK_RANGE setting?

Part Number: SN65DSI86
Other Parts Discussed in Thread: DLP3010, DLPC3433, TUSB1064

Our MIPI DSI source is from Qualcomm SD835, Dual MIPI DSI channels deliver two 1280x720x60 fps to SN65DSI86.

Our target device is dual DLP3010 projector, resolution is 1280x720 x 2pcs. and In DLP3010 spec, MIPI DSI data speed Max. is 470Mbps. so DSI clock Max. is 235MHz.

Please help confirm:

  1. Can we use 223MHz of DSI CLK when we use DSI CLK for CLOCK source of SN65DSI86.
  2. If we can use 223MHz of DSI CLK for Clock source of SN65DSI86, How to use that??

Should we use GPIO setting CLOCK(384MHz) for CLOCK source select? And then, we change the DSI CLK Range to 223MHz and re-send the DSI CLK?

All video path as below:

Qualcomm's SD835 => TI's SN65DSI86 => TI's TUSB1046 => TI's TUSB1064 => Toshiba's TC358860XBG => TI's DLPC3433 => TI's DLP3010 AR Display

In Display port, we use 2560x720x60fps setting. FYR.