Part Number: TPS65983B
Other Parts Discussed in Thread: TPS65987D, TPS65982-EVM, TPS65987DDJ, TPS65988
How to set up TPS65983B to be powered from USBC cable and being a power source for the customer circuit?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS65983B
Other Parts Discussed in Thread: TPS65987D, TPS65982-EVM, TPS65987DDJ, TPS65988
How to set up TPS65983B to be powered from USBC cable and being a power source for the customer circuit?
HI Michael,
Do you have access to the latest TPS65983B Application Configuration Tool? If not you will need to apply using the link from the Product Folder.
The TPS65983B is constrained to follow Intel Thunderbolt Reference designs and these constraints are defined in the Application Configuration Tool. You may use the Tool is modify allowed Source and Sink capabilities. These settings will define how the PD Controller offers and accepts PD Power Contracts.
Regards,
Scott
Hi Scott
thank you so much for your reply. i found the TPS6598X Application Configuration Tool from TI. does it support TPS65983B? where can i purchase the hardware/download cable?
thanks
Hi Michael,
First I want to check that you are using TPS65983B in an Intel Thunderbolt reference design. If this is not such a design, then you should switch to a different device, such as TPS65987D, that is not constrained to Thunderbolt reference designs.
Next, make sure you are using the Application Configuration tool specifically made for the TPS65983B. It can be found in the Secure Software folder after you obtain access. There are other versions of the Tool for parts other than the '83B.
The Tool will generate configured Firmware for the '83B. If this is a Thunderbolt reference design, the Firmware may need to be merged into the system firmware and then flashed or downloaded.
Also you will want to check the Firmware Users's guide on the TPS65983B Secure Software folder.
First I want to check that you are using TPS65983B in an Intel Thunderbolt reference design. If this is not such a design, then you should switch to a different device, such as TPS65987D, that is not constrained to Thunderbolt reference designs.
yes, i am using the TPS65983B in an Intel Thunderbolt reference design.
Next, make sure you are using the Application Configuration tool specifically made for the TPS65983B. It can be found in the Secure Software folder after you obtain access. There are other versions of the Tool for parts other than the '83B.
i filled up the request last week for the access and haven't heard anything back yet. Can you please help?
The Tool will generate configured Firmware for the '83B. If this is a Thunderbolt reference design, the Firmware may need to be merged into the system firmware and then flashed or downloaded.
Also you will want to check the Firmware Users's guide on the TPS65983B Secure Software folder.
Hi Michael,
Could you double check the My Secure Software link on ti.com? Right now I show that you have been granted access to the TPS65983B Design folder.
Regards,
Scott
Hi Scott
I found the TPS6598X configuration tool and clicked the "Get Software". The page then shows it is not available anymore.
can you please help? can I have your email address? I can't attach screen shot here.
thank you.
Hi Michael,
The tools for TPS65983B are separate from other PD Controller tools. I show you as having access to the correct design folder. Please try this and let me know if it works.
1. Go to www.ti.com
2. Check in the upper right for your login. Login with your email and password if you are not already.
3. Access the link for myTI.
4. Under the heading My Activity, look for a link to mySecure Software. This link should take you to the TPS65983 Design Resources. It should look something like this:
Let me know if this does not work.
Regards,
Scott
HI Michael,
No, there are no TPS65983B Evaluation boards available on ti.com.
It is assumed that the TPS65983B device will be placed on one of the supported Thunderbolt reference designs and that the USB PD portion of the reference design will be implemented exactly as specified.
Other TI USB PD controllers do have eval boards available for purchase. Some examples are the TPS65982-EVM and TPS65987EVM.
Regards,
Scott
Hi Scott
can I use the TPS65987D for thunderbolt application? what is the major differences between 65983B and 65987D? Please advise. Can I have a conference call with you to talk about my application?
thanks
HI Michael,
Yes, Intel has Thunderbolt reference designs for the TPS65987D and TPS65988. You will want to request special access to additional design resources from the TPS65987DDJ product folder.
A headline difference is the addition of support for 5A on the internal power path. I am happy to answer questions but cannot support a direct call. Are you in touch with local TI support?
Regards,
Scott
how can I request the additional design resources from the TPS65987DDJ product folder?
From the TPS65987DDJ product folder http://www.ti.com/product/TPS65987DDJ
Look for the link under More Information to request access to the Secure Software design resources. Start with this information and let's go from there.
Regards,
Scott