Part Number: TLK2711-SP
From the TLK2711-SP datasheet, there's a limitation cited where an unpowered receiver should not be driven by an external transmitter for more than 10 hours cumulative over the lifetime of the device. Does this same limitation apply to a powered receiver which has the ENABLE pin driven low (so that the device is powered, but disabled)?
It appears the ENABLE pin doesn't affect functionality of the high-speed serial receiver, just the parallel output (RXDn), but I wanted to confirm.
Thanks!