This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB934-Q1: Can UB934 works with UB935?

Part Number: DS90UB934-Q1

Hi team,

Is it possible to connect CSI camera sensor to UB935 serializer, and then deserialize ot with UB934 deserializer to connect to 12bit parallel camera input port at MPU side?

Like this: Camera => CSI-2 => UB935 => FPD-Link III => UB934 => 12 bit => MPU