This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TFP401: 4.3" 800x480 LCD panel can be used with TFP401?

Part Number: TFP401


Hello,

Customer wants to use TFP401 with 4.3" 800x480 LCD.

Is it possible to use without any setting?

Regards,

Nicky