This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB935-Q1: Details of format supported for Pattern generation in serializer.

Part Number: DS90UB935-Q1


Hi ,

I have a same query but for different serializer chip i.e DS90UB935-Q1 .

I want to use pattern generation with same configuration as mentioned  in section 7.6.4 .

But I want edit format from RGB888 to YUV. 

Ques 1:- Is YUV as output format for pattern is supported in this chip.

Ques 2:- Do i need to configure PGEN_CSI_DI register for this purpose .

If yes what is value for YUV422 format as, 0x24 is mentioned for RGB888.

Ques 3:-Please let me know all other formats which are supported with their hex values as they are not mentioned in data sheet.

Thanks 

Vishal