Part Number: TPS65988
Other Parts Discussed in Thread: BQ25703
hi Team,
customer using TPS65988 with bq25703 buck-boost charger. on a power bank design.
it's observed when provide power to a system board, after handshake, the VBUS is raised to 20V. however, when system power on button is pushed and starts to drain current. it's observed that the TPS76988 will trigger OCP and trigger HW RESET, but the loading is only 1.5A while the OCP threshold is ~3A.
it's observed that the system loading can have ~-200mA reverse current with the loading.
the PDIC FW version F407.06.15
we'd like to check.
1. what are the conditions that TPS65988 will trigger OCP.
2. whats the detection time and delay time when TPS65988 turns off the voltage output
3. when TPS65988 turns off the voltage output, will it proceed with a step down manner?
4. there was a fix implemented in FW to "reduce RCP sensitivity for Samsung phone's when there is transient reverse current" what is the negative current threshold?
Please check below image. Yellow line is voltage for VBus and blue one is voltage of BQ25703.
You can see that blue line keeps 20V when yellow line is decreasing. The Max./Min. current are 1.18A/-0.21A
MCU keeps BQ25703 to output 20V but 988D seems to close it MOSs.