This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS25BR100: Signal Integrity

Part Number: DS25BR100


Hi,

We are using DS25BR100  to drive LVDS signal for 1meter cable.

While doing signal integrity with cable we are checking the LVDS waveform after 1 meter cable and it shows the amplitude is lower than expected in LVDS.

Following is the setup which we have used to simulate the signals. While seeing waveform at the second buffer input it is showing lvds signals amplitude 100mV  and it should be 400mV.

Please help me out to understand why this happen at the input of second LVDS Buffer.