Part Number: TL16C2552
Hi team.
Our customer are replacing PC16552 to TL16C2552 .
We understand the difference is the MCR bit3 between them.
According to datasheet at p.23 and p.28.
On p.23, it is written 'Parity Enable'
On p.28, it is written 'Bit 3: This bit (OUT2) controls the high-impedance state output buffer for the INT signal and the OP output.'.
Is it correct TL16C2552's MCR bit3 is interrupt ?
And then,
If PC16552' MCR bit 3 is High, what does it do?
Sincerely.
Kengo.