Part Number: DS15BA101
Other Parts Discussed in Thread: DS25CP104A
Dear Technical Support Team,
Can I adjust the differential output swing = 550mV with Rvo?
I guess that Rvo = 824Ω means 550mV, right?
If you have the data of differential output swing between Rvo= 487Ω(800mV) to Rvo=953(400mV), could you share it?
In addition, Is Output Common mode voltage =0.825V(Vcc-Vout/2) when Vout = 550mV with Vcc=1.1V?
My target is "Output Common mode voltage = 0.55V" and "differential output swing = 550mV" with Vcc=1.1V.
Best Regards,
ttd