This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMH0318: Can LMH0318 accept DS25CP104A LVDS output ?

Guru 19785 points

Part Number: LMH0318
Other Parts Discussed in Thread: DS25CP104A,

Hi Team,

I have a question about LMH0318 whether it could accept DS25CP104A LVDS signal.

Please see the following specification.
The unit is different from each other which is mVp-p vs mV.

LMH0318 is described as "peak-to-peak voltage", however, DS25CP104A is not.
Does the Launch amplitude of 500mVp-p mean 250mV differential ?

If it is correct, I believe LMH0318 could accept LVDS signal with AC coupling.  

[LMH0318 Input Specification]

[DS25CP104A Output Specification]

Best Regards,

Kawai