Part Number: TPS65987DDJ
Other Parts Discussed in Thread: TPS65987D
Hi Team,
In my customer design, as it is a monitor, we set the port as DRP with TrySrc, and select the following setting.
However, in PD3 certification test, there is a test that the tester will test the DUT to be a sink, and will force a current to the DUT. In this case, as the monitor is a sourcing only, and will not sink current, we did not check the "process swap to sink", and it will fail the test, and should get a wavier.
My customer would like to know the behavior if we check the "process swap to sink", what will be the behavior that we could expect?
Another question is regarding the "Process Vconn swap". If we uncheck this, do we expect that during initial plug-in, the PD will not provide the 5V to Vconn? or it is just do not process the Vconn swap request when the platform wanted to pass back the Vconn to the PD?
Regards
SK Loo