Part Number: P82B715
Hello.,
BUFFER IC VCC 3.3V
and MASTER is 3V, I2C PULL-HIGH was 3V also
then through 715 to SLAVE side PULL-HIGH all 3.3V
is there any concern for the application, thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: P82B715
Hello.,
BUFFER IC VCC 3.3V
and MASTER is 3V, I2C PULL-HIGH was 3V also
then through 715 to SLAVE side PULL-HIGH all 3.3V
is there any concern for the application, thanks
Hi Philip,
This isn't typical usage of the device, but it may work (especially given that the voltage difference is small and the bus voltages will not exceed VCC). We will examine this in more detail and get back to you later in the week to confirm.
Max
Hi Philip,
The P82B715 Lx and Ly connections are clamped at Vcc +.07v but are otherwise independent of the supply voltage. As long as the bus voltage does not exceed Vcc by this margin and Vcc is within the datasheet specifications, the device should operate as normal.
Reduced performance will occur with Vcc < 4.5v. This mainly impacts the dynamic sink currents and requires accommodation for timing-critical designs. Let me know if you have any questions regarding this trait.
Regards,
Eric