Part Number: DS90UB947-Q1
hello,
For the 0x5C[2:0] FREQ_HYST setting, if the clock frequency is over the setting, what will happen? Lose lock?
Can we set 0x5C[2:0]=0x03 to improve the hysteresis? Thanks.
Dongbao
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB947-Q1
hello,
For the 0x5C[2:0] FREQ_HYST setting, if the clock frequency is over the setting, what will happen? Lose lock?
Can we set 0x5C[2:0]=0x03 to improve the hysteresis? Thanks.
Dongbao
hello Dongbao,
if you write 0x03 instead of 0x02 then you are increasing the window of allowed fluctuations in the frequency.
Hi Hamzeh,
What will happen if the clock frequency is over the 0x5C[2:0] FREQ_HYST setting,? Lose lock?
Thanks.
Dongbao
If the clock frequency is outside the Hysteresis range the freq_stable signal will be deasserted.