I've few question integrating MSP432 series with CAN Transceiver like MAX14883E/ADM3055E/SN65HVDA1040B/ATA6563.
As per the Data sheet, MSP series controller doesn't support CAN since they don't CAN Controller.
I believe using CAN Controller like MCP2515 and CAN Transceivers It's able achieve.
But are there any CAN Controller from TI(may be integrated Transceivers?).
And also as per the data sheet attached below, in Page No 10, Image shows Controller can be directly connected to CAN Transceivers using UART, Is it meaning that CAN Controller?

Thanks.