Part Number: PCA9306
Can the PCA9306 be used in a configuration where VCC2 is lower then VCC1. VCC1 = 3.3V and VCC2 = 2.5. The 3.3V side is the host side and the 2.5V side can/will be powered down. Is there another device I should be using or should I simply flip the part. I can disable the part with daughter board reset which is driven from the 3.3V side.
Thanks.