Part Number: XIO2213B
Hi Sir,
Our customer want to use the XIO2213B, need EVM layout file to design.
Could you please share for me?
Hugo
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello-
The XIO2213B EVM, designed as a x1 add-in card, is routed on FR4 with a standard 4-layer board with 100 Ohm differential impedance (For PCI-Express differential pairs), 110 Ohm differential impedance (For 1394b pairs), and 50 Ohm single-ended impedance using routing guidelines and requirements specified in the PCI Express Card Electro-mechanical Specification rev 1.0a, PCI Local Bus Specification rev 2.3 and IEEE 1394b-2002.
Best regards,
Davor
Hi Sir,
Do you have XIO2213BZAY layout file can be share for me? example *.brd
As below link have XIO2213ZAY REFERENCE DESIGN,But this is PDF file.
Do you have XIO2213BZAY DSN file can be share for me?
https://e2e.ti.com/support/interface/f/138/t/766493
Hugo
We no longer have the DSN file but please find the .brd file attached below:
Regards,
I.K.