Part Number: TPS65988DJ
Hi Sirs,
Sorry to bother you.
Could you help review our schematic as below?
Any suggestion are welcome.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS65988DJ
Hi Sirs,
Sorry to bother you.
Could you help review our schematic as below?
Any suggestion are welcome.
Hi Shu-Cheng,
I will check your schematic design and get back to you tomorrow on my suggestions.
Thank you,
Hari
Hi Shu-Cheng Lin,
I have looked at the schematic and it looks fine for the most part. I do have some recommendations though.
- I recommend reconfiguring the pins "BB0_LS_EN" and "USB_OC0#_PCH" from GPIO 12 and 13 to GPIO 16 and 17.
- I also recommend pulling up the I2C2 pins to LDO_3V3 since they are being used.
Thank you,
Hari
Hi Sirs,
Thanks for your reply.
Update schematic as below. Please let me know if have any risk on our design.
BB1_LS_EN" and "TC_RETIMER_FORCE_PWR" from GPIO 14 and 15 to GPIO 16 and 17
I2C2 Pull High 2.2K to PDf 3V3
Hi Shu-Cheng LIN,
I edited my last comment just a few moments after I replied to say GPIO 12 and 13 instead of 14 and 15. So, I would recommend changing the GPIO pins 14 and 15 back to what they were previously and then reconfiguring GPIO 12 and 13 to GPIO 16 and 17.
Additionally, I noticed that your other I2C1 and I2C3 pins are connected to +3VSUS. I would recommend pulling up ALL of the other I2C ports and pins to the same LDO_3V3 net as well, the way you did for I2C2.
Other than those 2 changes, I think your schematic looks good.
Thank you,
Hari
Hi Sirs,
Thanks for your reply.
Actually this project has been mapped on last Fri, so can the settings of these GPIOs be adjusted through the tool?
Thanks!!
Hi Shu-Cheng LIN,
The GPIOs cannot be reconfigured through the GUI if that's what you are asking. You could test those GPIO pins from the design and see if it still functions as planned to be certain.
Thank you,
Hari