Part Number: TL16C2550
HI, staff
I have a question about the falling timing of _CSA and _CSB of TL16C2550.
Used at 3.3V.
What is the meaning of the time specified in data sheet page13 td5 and td8?
1. After addressing, the transition time of _CSA and _CSB fall time should be at least 7ns.
2. After addressing, the fall time of _CSA and _CSB is changed within 7ns at the minimum.
Which of the above “1” or “2” is correct?
Can td5 and td8 be "0nsec" (simultaneous transition)?
best regards
cafain