Part Number: TVS0701
Hi,
my customer needs 5V USB power line TVS, but the
IEC 61000-4-5 Current (8/20 µs), TA < 125°C
need to be at least 100A.
It seems that all our TVS current are less than 100A.
Do we plan to release higher current TVS?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TVS0701
Hi,
my customer needs 5V USB power line TVS, but the
IEC 61000-4-5 Current (8/20 µs), TA < 125°C
need to be at least 100A.
It seems that all our TVS current are less than 100A.
Do we plan to release higher current TVS?
Hello.
What voltage would you like to clamp to?
Our clamping voltage is much Lowe than competition that allows lower power dissipation
Less than 20V.
In fact, this question is not related to this device only.
I'm just curious are we going to release higher current devices in the future. It seems that our biggest current of all TVS is only 40A.
Hello,
As of right now we are only planning to have these TVS devices for surge protection