This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN1042-Q1: ISO26262

Part Number: TCAN1042-Q1
Other Parts Discussed in Thread: TCAN4550-Q1, TCAN1043

Is TCAN1042-Q1 qualified for QM according to ISO26262?

Thanks

Viktorija

  • Viktorija,

    The only device we have ASIL QM documentation is the TCAN4550-Q1 because it has fault-detection with external indication and some kind of control of the system. The TCAN1043 could also be somewhat considered for this rating, but the TCAN1042 has no control or indication of faults, just self-detection.

    For the TCAN1042, we can provide the failure mode distribution and the pin FMEA to show fault and failure conditions. Would this help?

    Regards,